XP Power
Blog

History of Switch Mode Power Supplies (SMPS)

Posted by XP Power on 10-May-2016 14:30:00

Tags: SMPS

GCS350I recently had lunch with a customer we’ve worked with since the late 1990s. We’ve seen a lot of change in that time and, as the main course arrived, we started talking about how power supply technology has advanced over the years. This has been most noticeable in the areas of efficiency and power density. 

The first ever unit he designed using XP Power was a 3 x 5" 40W PSU. That might have been considered revolutionary at the time but when you consider that his most recent product used a 350W unit in the same space envelope, it becomes clear just how far we’ve come.

I’ve done a little research on this following our working lunch and, as far as I can tell, the very first switch mode power supplies were designed in 1958 by IBM. They were based on vacuum tube technology. Several patents were filed for a ‘transistor oscillation’ by General Motors Corporation around the same time. With this influx of technological advancement, designers were suddenly able to pick and choose from multiple components and multiple manufacturers, giving them an unprecedented number of options and potentially groundbreaking designs.

The focus of this intensive period of development was the traditional linear regulator – the brightest minds were trying to figure out how they could replace the outdated transformer and resistance method of changing input voltage with a more efficient design.

The idea they landed on used a transistor to chop the input voltage up with an average value less than the initial input (we have a fantastic store of technical articles here on the site if you’d like a more detailed description of SMPS operation). With higher efficiency and fewer magnetic materials required, the new technology was smaller, lighter and generated less heat. As with modern inventions with those characteristics, this 1950s solution was hugely appealing to businesses in a range of sectors – from electronics to aerospace and communications to computing, there was a flood of early adopters each jockeying to make the best use of this new power supply technology.

Over the next few years a flurry of patents and designs emerged - many of which we still use today. In 1972, Hewlett Packard used a switching power supply in its first pocket calculator. 1976 saw the first patent to use the term switch mode power supply (SMPS) filed.

HP’s calculator was really a computer – albeit in a slightly different format than we know it today. Back then, the original design weighed over 40lbs. The SMPS was used in the design to save both space and weight, marking the first step towards the ultra slim and incredibly light computers, laptops and tablets we use today. Similarly, aerospace manufacturers considering how they could save weight and space also began looking towards custom switching power supplies to create much more efficient designs. 

The 1970s was a busy decade once the initial breakthrough had been made and innovation continued at a very respectable pace. Several companies in UK, USA and Japan began to market standard power supply products. To this day, there are around a dozen companies who claim to have been the first to design and market a switch mode power supply successfully – so we won’t go there!

The electronics magazines of the era featured articles and adverts for SMPS. The leader at that time was Boschert Inc., an American corporation that started in California. It replaced linear printer power supplies with switch mode designs. This company grew to over 1000 people, with a vast product range of open frame, cased and modular power supplies. It was eventually acquired by Computer Products Inc in the mid 80s. 

Apple Computers first introduced a switch mode power supply into the Apple II computer in the 1970s. This small, highly efficient technology meant Apple could build a smaller, lighter computer without a cooling fan. This type of convection cooled design was unique at the time. The technology had taken on a life of its own and was used in dozens of consumer applications. IBM PC power supplies also made the move to switch mode, albeit with cooling fans similar to the ones they use in ATX style power supplies today. 

In the late 1980s and early part of the 1990s, we were stunned when the industry standard 3 x 5” power supplies became available with an auto-ranging input that sensed whether it was connected to 120VAC or 230VAC and adjusted accordingly. These products had powers of 25 – 40W, or 1.66 to 2.66W/In2

As more and more companies entered the market, some loose industry standards appeared around common sizes like 3x5”. Power densities began to improve as advances in magnetics, switching transistors and controller ICs progressed. These changes offered higher efficiencies and made better power densities possible.

By the early 90’s the W/In2 available from multiple sources had more than doubled. The EU stepped in with new legislation and Union wide directives that meant that more focus was placed on EMC emissions and the power factor of power supplies. Essentially as more and more products used the technology, there was more need to control electrical interference. Issues with the sizing of the conductors needed to deliver the power to where it was needed in the grid also played their part. 

The EU legislation was particularly disruptive to the SMPS market as switching technology is much noisier than linear power supplies. Additional circuitry was also needed to shape the input current waveforms to sinusoidal forms – this allowed them to meet the power factor requirement and prevent excess harmonics causing problems with the grid supply. 

So where are we today in terms of power density? Well, the customer I had lunch with just approved our latest 350W 3x5” power supply with a power density of 23 W/In2. This is more than 10 times the power of the first power supply he bought from me. What’s interesting is that thanks to the commercialisation of the technology, higher volumes and low cost Asian manufacturing, this product is available at a very similar price point to the earlier 40W units.

Power selector brochure

About the Author

XP Power is committed to being a leading provider of power solutions, including AC-DC power supplies and DC-DC converters. XP offers total quality, from in-house design in Asia, Europe and North America through to manufacturing facilities around the world.

XP Power